Change Language :
Prefabricated energy supply system in steel production
Heat and dust: these are just two of the components that arise during sheet metal production. There is also plenty of scale waste. In these harsh operating conditions, a preassembled energy supply system comes into its own. It can handle a travel distance of almost 100 metres, offers a long service life and thus guarantees operational reliability. The plastic energy supply system does not need to shy away from comparison with a comparable solution made of steel; it copes perfectly with the difficult environment.
"The potential is far from exhausted at voestalpine as a whole. Traditional steel fabricators, who naturally prefer to use steel energy supply systems, are learning about the advantages of plastic energy supply systems in this demanding application. With the pre-assembled version, we are also presenting ourselves as a complete supplier."
Dieter Bencer, Technical Sales Consultant, igus® polymer Innovationen GmbH
For many years, the engineering office has mainly relied on energy supply systems from igus® for its projects. "The potential is far from exhausted at voestalpine as a whole," Dieter Bencer points out. "Traditional steel fabricators, who naturally prefer to use energy supply systems made of steel, are learning about the advantages of energy supply systems made of plastic in this demanding application. With the pre-assembled version, we also present ourselves as a complete supplier." The complete energy chain system has also been tested in the igus® laboratory. "The customer has a comprehensive system guarantee on the guide trough, the energy supply system and the chainflex® cable used," confirms Dieter Bencer. "And should any technical problems arise, we can react quickly simply because of our geographical proximity to the end customer."
Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.