Lubrication-free and maintenance-free heavy-duty bearings in the chassis of new RTG cranes

Crane manufacturer Tan Cang Gantry installs lubrication-free bearings that do not require regular maintenance.

Profile

  • What was needed:
    Lubrication- and maintenance-free high load bearing " igutex ® TX",
    Roller-energy chain P4HD,
    chainflex® cable
  • Requirements:
    The customer was looking for bearing points that could support particularly high loads in the chassis of the RTG cranes, withstand harsh environmental conditions and reduce
  • maintenance work. Success for the customer : 
    The high-load bearings "TX1" offer a maximum permissible surface pressure of 200 MPa. The special feature: thanks to the inner layer optimised for sliding properties, they are friction-optimised, durable and completely lubrication- and maintenance-free. The customer can dispense with regular maintenance and at the same time increase safety during crane operation.
Chassis RTG crane

Tan Cang Gantry specialises in the manufacture and construction of port equipment such as RTG cranes.

As part of a co-operation with igus® Vietnam, Tan Cang Gantry relies on completely lubrication- and maintenance-free high-load bearing technology in the chassis of its RTG cranes, among other things.

The installed high-load bearings "igutex® TX1" consist of a robust glass fibre fabric in the outer shell. The maximum permissible surface pressure is up to 200 MPa.

Tan Cang Gantry also obtains the cable routing from igus®: A roller energy chain of type P4HD. "HD" describes the suitability of the unwinding chain for heavy-duty applications.

As the upper run of the roller-energy chain does not glide on the lower run "" but rolls, the frictional resistance when moving the chain is reduced to a minimum.

UL-approved chainflex® cables were selected for the guided cables. The UV-resistant chainflex® cables are specially designed for long travel distances in energy chains and narrow bend radii.

Assistance pour les demandes

Pour toute question supplémentaire ou information sur les produits, veuillez contacter :

igus® Inc. Canada+1 800 965 2496Courriel