Change Language :

Pharmacies that want to store their medicines in a particularly space-saving manner are best advised to contact Gollmann Kommissioniersysteme GmbH in Halle (Saale). The company uses the drawer cabinet system to efficiently store up to 60,000 packaging units in a small space and to pick them fully automatically. The company has been working successfully with us for more than ten years to select and optimise the moving cable and energy chain.
"So far, we have installed more than 20,000 energy chains in our order picking systems worldwide, and they run very reliably without any malfunctions or maintenance."
Sven Ronneberger, technical conductor at Gollmann Kommissioniersysteme GmbH
The innovative roller cabinet principle of the order picking systems has now aroused interest beyond the pharmaceutical industry. Sven Ronneberger: "We are increasingly planning systems for completely different applications - for example, for the management of tens of thousands of samples at a manufacturer of spice blends for the catering industry." In another case, a metalworking company stores expensive turning and milling tools in a Gollmann vending machine. If a tool is worn out, the worker - provided he has user authorisation - fetches a replacement, and the company can easily keep track of the service life of the tools. A completely new and rather exotic application is pop-up stores, which are set up in shopping centres, for example, and used as space-saving and attractive temporary sales outlets. Not only the Gollmann designers, but also the sales department are clearly not running out of ideas. In igus®, the company has found an equally agile partner for mobile energy and signal supply.
Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.