Change Language :

Plastic bearings are a crucial part of the design
This hydrogen-powered vehicle successfully completed a 1,864 mile-long European tour in 2004. The vehicle required only 7.3 lbs of hydrogen to cover the distance between Berlin and Barcelona. This corresponds to 3.2 gallons of gas and a consumption of 0.1 gallons per 62 miles. A prerequisite for the world-record attempt was to save as much weight as possible and, at the same time, to guarantee the reliability of the system. A crucial design engineering detail was rod end and plain bearings from igus®, which have a low mass and ideal mechanical properties.
Dirt-resistant and space-saving
The HTD belt connects the rear wheel and the engines with one another and is tightened with a tension pulley. This needed to be insensitive to dirt, as it is close to the ground. iglide® W300 plastic plain bearings were used, because they have a high compressive strength, are maintenance-free, vibration dampening and insensitive to dirt. They also have very low coefficients of friction and extremely high wear resistance.