Change Language :
From filling to palletising, products often have to pass through different areas. Within the further processing of goods, however, there are also critical points such as the fire protection sections. Fire dampers, which are used for compartmentalisation, must always be kept clear in the event of an alarm. ASH GmbH & Co KG has developed a so-called retraction conveyor belt for this purpose. This can be shortened, freeing up space for the fire protection systems. This system was realised with the help of igus® linear bearings and drylin® T guide carriages.
Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.