In future, the vegetable producer Reichenau-Gemüse will pack its tomatoes and apples in cardboard trays without film and therefore without any plastic. An S-shaped viewing slit allows a clear view of the product (see image 1 below).
This new product is made possible by the development work of Dipl.-Ing. Michael Baur. His company is active as a development service provider for special machine construction.
The starting point for the development was the wish of a corrugated cardboard manufacturer to dispense with the usual flow-wrapping and thus the use of plastic foil. The company launched a tender for an ideas competition, which Michael Baur won. The challenge: gluing without backing and without pressure on the product. In the next step, Michael Baur and his team built a prototype of the newly designed machine. One of the particular challenges here was to glue the printed packaging to the top after it had been manually filled with vine tomatoes: The bonding must be durable. During the gluing process, however, it is not possible to apply any pressure to the sensitive tomatoes. This task was solved by an intelligent detailed design. The glue dots are applied using a hot glue station, but other methods, e.g. sealing are also possible. Sealing is also conceivable. A station for printing and applying the labels is also integrated into the system. When developing the prototype, Michael Baur placed great emphasis on flexibility and ease of operation. This can be recognised at first glance by the numerous semi-automatic format adjustments (picture 2).