But since switching over to iglide® bushings, his Ripmo V2 has proven to be extremely robust in difficult mountain terrain. "In over two years of riding, our Enduro Team hasn’t broken any bushings", says Wallner. "They have definitely been holding together better than I originally thought. They are also lighter and much easier to maintain than the bushings I previously used."
Wallner is one of the world's very best bike riders, at whom development is actually aimed. "All mountain biking technology is developed for use in racing, with speed in mind", says Matt Floyd, igus® sales manager for the west region of the USA. "Most of the technology, however, is used by recreation cyclists." And they will also be pleased if lighter bearings that have a long service life and do not have to be maintained are used in the bike.