Change Language :
Transmitting data volumes quickly and without interference
The technical requirements for energy supply systems in mechanical and plant engineering demand functionally reliable cables. igus® The company , Cologne, is increasingly relying on glass fibre optic cables, which allow very high data volumes with increasing cable lengths. The "chainflex® CFLG.2HG" product family is now available as sold by the metre or assembled with connectors from stock.

Fibre optic cable endurance test in the igus®® laboratory: 60,000 kilometres covered in the energy chain without interference.
The glass fibre optic cable of the CFLG.2HG series was also tested for two years in the igus®® energy chain laboratory. A travel of 2 m with a bend radius of only 100 mm and a speed of 2.5 m/s was selected. Even after more than 30 million movements in the energy chain - that is 60,000 kilometres - no technically relevant increases in attenuation were detected. The end of the test is not yet in sight.
Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.