Change Language :
A freshly baked pizza in just 90 seconds at the touch of a button? The BistroBox is a self-service pizzeria with Austria's first fully automatic pizza oven. The centrepiece of the innovative combination of refrigerated storage system and pizza oven is lubrication-free and maintenance-free bearing technology such as a belt conveyor and other bearing technology that ensures the pizza is transported from the cooling station to the oven and finally to the customer. All components must fulfil the high hygiene requirements in food technology ... at temperatures of up to 300°C.




Picture 3: The platform with the pizza, which travels along the toothed belt axis, can be pulled out. 3D-printed gears and gear racks help here.

Picture 4: In this station, the pizza is freed from its packaging. The platform in the station rotates around its own axis several times. This is made possible by a PRT slewing ring bearing.

Picture 5: igubal clevis joint with spring-loaded fixing clip work in the closing mechanism of the oven door.

Picture 6: The FDA-compliant blue tribotape liner reduces wear at friction points within the vending machine.

Picture 7: Low-friction bearing: xiros ball bearing in the vending machine.
Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.