Change Language :

The two fully automatic tyre fitting lines at MC Syncro Supply GmbH fit a tyre onto a rim in an average of approx. 7.5 seconds each. The lines usually run 5 days a week in a 3-shift system, which corresponds to around 120 hours per week. At the so-called tyre soap station, the diameter of the tyre is determined from the inside and the inner bead of the tyre is wetted with soap using brushes. This runs into the brushes from above and the excess flows back into the storage container via a trough. The tyre is transported to and from the tyre soap station via toothed belts mounted on two brass shafts.
The medium soap washes out the grease over time, even from encapsulated bearings. Especially with metal bearings, lubrication with grease or oil is essential for a long service life and optimum bearing performance in machine operation.
As soon as the grease had washed out, the metal bearings jammed and the shaft continued to rotate, causing it to run in within a very short time. The damage: approx. 6 hours repair time and replacement of all defective components (2 shafts, 4 bearings, 2 toothed belts) at a cost of 610 Eurp. This repair had to be carried out twice a year per machine. The costs for the repairs and the machine downtime were therefore several thousand euros.