Change Language :

The company Produtek Weiskopf uses two side-by-side injection moulding machines in which plastic parts are injection moulded from three components. A joining station is located between the two machines. Here, the second component, a viewing window, is inserted into the basic component from the first machine. The assembled parts are then transported onto a cooling belt and from there to the second injection moulding machine, where the third, soft component is injected.
Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.