This is where the lubrication incorporated into iglidur® sliding elements pays off. The solid lubricants are microscopic particles embedded in millions of tiny chambers in the material, which is usually fibre-reinforced. From these chambers, the plain bearings release tiny amounts of solid lubricants during movement. This is adequate to sufficiently lubricate the immediate surrounding area.
 
In addition to the drylin® W guide system, tribo-optimised polymer plain bearings are used in the grippers. They replace aluminium plain bearings, which were very expensive to procure and then required machining because they were not available in the required dimensions. "The polymer plain bearing cost is unbeatable, and the bearings can be used right away", Geisler says. "You open the bag, insert the bearing, and that's all there is to it."
 
iglidur®: low coefficient of friction, minimal wear
The lubricants help to reduce the igus® bearings' coefficient of friction. They are not indispensable for the bearing's function, but have a supporting effect. Since they are embedded in the tiny chambers, they cannot be forced out. They are always there as soon as the bearing or the shaft is set in motion. The lubrication is protected from outside contamination for as long as possible, which means it can always be counted on for its full effect. The material used in this example is iglidur® J200, which has been specially developed for a very low coefficient of friction and minimal wear on hard anodised aluminium shafts. In this context too, raw materials savings, which is part of environmental concerns, plays an important role. Just as the welding cap change is performed very precisely, the guide system requires no additional lubrication, with positive effects on the net environmental impact. "The system can be relied upon for long and continuous operation. No maintenance work on the guide is necessary after installation", says Geisler.