Change Language :

For an optimal feel of the unique rotary knob, much attention has been paid to the search for the optimal material for the bearing in the new generation of household appliances.
Over 100 years ago, V-Zug set itself the task of making everyday life easier with high-quality, innovative household appliances. The company has been family-owned since it was founded in 1913 and is one of the most important employers in the canton of Zug. With state-of-the-art working methods and over 1,400 employees, the high-tech company develops and produces high-quality household appliances in Switzerland. Over 4.5 million appliances are in use throughout the country. On an area of over 60,000 square meters, V-Zug AG manufactures household appliances for the kitchen and laundry room with the highest precision and pioneering production techniques, from the basic material to the finished appliance.

Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.