Change Language :
Heineken is a global powerhouse in the world of brewing. It’s the largest beer company in Europe, and the second-largest in the world. Heineken generates tens of billions of dollars a year in revenue, and is an industry leader when it comes to tech infrastructure and sustainability.
Heineken’s Brazilian location (Heineken Brasil) is one of the brand’s largest, and a leader among the company in renewable energy. As part of Heineken Brasil’s environmental focus, they began looking for ways to mitigate their use of lubricants in bottling conveyor belts.
Heineken Brasil needed an updated solution for conveyor belt bearings. The metal bearings used initially required relubrication on a weekly basis. With 600 bearings — each requiring three minutes of lubrication time per week — Heineken was losing 1,560 hours of time a year just to relubrication.
In searching for a cleaner, lower-maintenance solution, Heineken Brasil came across igus’ dry-running igubal JEM insert bearings. These plastic bearings operate without the use of any lubricating greases or oils, offering maintenance-free and food-safe operation.
The selected insert bearings made replacement a simple drop-in process, minimizing the time needed to replace each bearing and ensuring no special training or installation assistance was needed.

Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.