Change Language :

BANG Kransysteme GmbH & Co. KG in Oelsnitz/Vogtland is successful throughout Europe with its process and special cranes. The cranes deliver top performance, for example in the steel industry, in the pressing plants of the automotive industry and also in the area of nuclear facilities. With a current project, the company is showing that it can also do standard - and then flexibly go beyond the standard when the need arises. This is why our new autoglide 5 energy chain is being used in the new overhead crane at ZSB Zwickauer Sonderstahlbau GmbH.
"We are very satisfied with both the cranes and the project schedule, and the new channel-free energy chain is proving its worth."
Peter Knösel, Head of Project Management and Sales at ZSB Zwickauer Sonderstahlbau GmbH
Tech up ... Reduce costs.
In this igus® magazine you will find numerous possibilities and application examples of how you can reduce tech up and / or costs with ready-to-install energy chain systems.

Service clientèle:
Téléphone : du lundi au vendredi, de 8 h à 17 h.
LiveChat : 24 heures sur 24.
Prendre rendez-vous
Prendre rendez-vous avec un expert produit.