Watering machines are used in horticulture to supply plants with water, as well as the nutrients dissolved therein. In order to be able to reduce the application and use of irrigation water to just the necessary level, Dercks Gartenbau GmbH has developed the "precision watering" machine. The idea behind this is to give the plants exactly as much water as they need to grow.
With this irrigation system, the company is able to precisely apply the irrigation water to the center of the pot. However, on the farm's potted plants on around 8 hectares (almost 20 acres) of open land, there is not only a great potential for saving water. In addition to a 35% reduction of the amount of water that would otherwise have to be brought to the watering machines, the electricity consumption required to operate the pumps can also be reduced by about half.
Based on the idea in spring 2015, a first prototype for the precision watering machine was constructed, which operates on a floor space of 2,400m2 and supplies plants in larger planters with a low population density. Based on the positive experiences, another, significantly larger model was finally developed in 2018. The prototype watering machine has a span of 45m, reaches a travel speed of 18m/min and covers an area of 9,180m2. At 32 pots per m2, the precision watering trolley achieves a water saving potential of around 60%. In total, over 4,000 cubic meters of irrigation water and over 1,400kg of nutrient salt can be saved per hectare and season.
In order to be able to safely carry the supply cables - specifically the two 1 1/4" hoses for the water supply - for the long travel distances of the irrigation system, the horticultural company was looking for suitable cable guide.