Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Automatic punching machine
For rolling shutter sidebars
Order a free sample

Technical data:

  • What was needed: A machine that punches holes in rolling shutter sidebars and can automatically adjust their position
  • Requirements: Space-saving; fast, precise movements, even with automatic instead of manual punching; special lead screw nut designs
  • Products used: dryspin® DS10x25 high helix lead screws, dryspin® DS10x25 lead screw nuts (special design), drylin® WW complete carriages, drylin® W double rail, motor flange for stepper and DC motors, drylin® E elastomer couplings
     
  • Success for the customer: The application axis completely automates the punching process. The use of a single axis also reduces costs and required space. 
Aircraft throttle

Punching machine application description

From Roto Okna Dachowe

Describe your system/machine/project. What is the function of your application? Where is your application used?
Our application is a device for punching holes in rolling shutter sidebars. The machine consists of four punching tools, three movable and one fixed. The punching machine is used to automatically move these punches to the desired positions with a control system and stepper motors. Three carriages on one axis move the punching tools to the desired positions in a fast, space-saving, precise and repeatable manner. 

What are the usage/environmental conditions at the end user's location? What requirements had to be met to adapt to those conditions?
The small installation space requires a compact solution. The application is used in a device for punching holes in rolling shutter sidebars, so the system had to be positioned precisely.

Which polymer bearing technology solutions do you use?
A 1.5-metre ​​​​​drylin® W WS-10-120 double rail and three drylin® W WW-10-120-10 complete carriages. There are also three dryspin® high helix lead screws measuring 10x25 with matching lead screw nuts, a special design. Propeller mounts with mountable motor flanges for stepper and DC motors (MF-2040-NEMA23-S) and drylin® E elastomer couplings were also installed. The application axis completely automates the punching process. The use of a single axis also reduces costs and the space required.

At which points? How did the products solve your problems?
The applied axis, coupled with the punch holders, completely automates the punching process. After the default values are entered, all punching tools move much faster and more precisely to the specified positions than they would with manual work - errors are eliminated completely. Using a single axis significantly reduces costs and makes installation easy with a very small system footprint.

How did the cooperation with igus work?
I have been using igus products for several years and know the these systems' capabilities. When I presented my idea to my igus consultant, it turned out that, although the system I wanted was available, it was new and therefore not listed in the online catalogue. I received drawings and all information about the product. I told him my requirements, and the result was a product that was tailored to the needs of my application.

Punching machine

Further application pictures

Punching machine
Lead screw nut
Punching machine

Products used

High helix lead screw

Lead Screw

dryspin® high helix lead screw nut

Lead screw nut

Flange for stepper and DC motors

Motor flange

drylin® W WS double rail

Double rail

drylin® W WW complete carriage

RJIP

Do you have questions about drylin® lead screw technology?

Our expert Thorben Hendricks will answer all your questions about drylin lead screw technology. Just fill out the contact form and we will take care of your issue. We are looking forward to your message!

► Request contact online
► Make an appointment
► Expert support upon request by phone or with the video chat function
► Order a free sample
 
Request expert support here

Configure lead screw drive:

Filling system

Improve technology ... reduce costs:

Tech up, Cost down



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG