Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Temperature-resistant cables in LED monitor
Energy supply system in spite of heat, sun, rain and snow

The cables from a competitor which were used earlier had collapsed.

The cables used before retrofitting could not withstand the existing temperatures of -5 degrees Celsius. Since the temperature resistant chainflex® cables have been used, the larger-than-life LED screen at Victory Plaza in Dallas works in heat, sun, rain and snow.
To ensure the high data volume for perfect images even after several million cycles, the temperature-resistant CFLG.6G chainflex® fibre optic cables are being used in the facility in Dallas, which can be operated even at temperatures of -40 degrees Celsius. The cables are successfully tested at the igus® test lab in Cologne for over 20m in the energy chain. Just as the fiber optic cables, the chainflex® control and motor cables also fulfill the high requirements in terms of temperature and low abrasion. They were successfully tested at igus® for millions of cycles.
Temperature-resistant chainflex® cables were used in an LED screen at the Victory Plaza in Dallas.
temperature-resistant chainflex® cables in energy chain

More on applied products here

Further interesting applications from extremely diverse areas can be found here.



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG