Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Gripper system

This application is a screw head with four bearing positions for gripper arms, which can spread their fingers via compressed air cylinder. The bearing was not first in the foreground, but the format part of the screw head, which should be manufactured in the FDM-technique. First tests with standard filaments like PLA or ABS failed because they do not have the required material properties. The breakthrough came with iglidur® I150. Now the screw heads are extremely stable but have a high elasticity at the same time, which simultaneously prevent breakage of the parts. Format parts are generally very cost-intensive in the Health Care and pharmaceutical industries and require a longer planning phase, which limit the flexibility of the companies. It is now possible to react much faster onto the customer’s desires duet to the changed procedure – accompanied with a cost-reduction of 85%.
gripper system
gripper system

Carecos Kosmetik GmbH, Heiko Meier, Kehl, Germany

Here, you can find the products used

Here you can find further interesting applications from very different areas of use:

Go to manus® competition



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG