Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Shore-side power supply of FSU/FSRU at Liquefied Natural Gas Terminal (LNG)


Shore-side power cable management system for floating storage unit in Bahrain

For the new offshore LNG terminal in Bahrain, Schneider Electric  and igus have developed the world's first shore-side power supply system for a Floating Storage Unit (FSU). The core component of the system is a flexible cable feed system that bridges the 30 m distance between the crossbar and the FSU.

Profile

  • What was needed: Heavy-duty energy chain for the offshore sector. Emergency shutdown system
  • Requirements: Flexible energy supply due to the FSU often being in heavy motion, harsh environmental conditions required an emergency shutdown function for the whole system
  • Industry: Shipping
  • Success for the customer: State-of-the-art energy supply solution, low-maintenance and safe despite difficult environmental conditions
Application Schneider

Problem

Liquefied Natural Gas (LNG) is one of the most important energy sources of the present and future, as it emits only very small amounts of greenhouse gases and is therefore considered an important fossil fuel. In Bahrain, the state authorities have set up a joint venture for the planning and construction of an LNG terminal, which has just gone into operation.
Due to security requirements, the terminal is located at sea, about three kilometres off the coast. The LNG tankers dock at the jetty and release the natural gas into a so-called Floating Storage Unit (FSU), which later pumps the gas via underwater pipelines to a regasification unit on shore.
Schneider Electric was responsible for the entire energy infrastructure in this project. In order to supply the floating storage unit with power, a connection had to be created between the terminal and the FSU. Here not only a distance of more than 30 m had to be bridged, but also the movements of the FSU due to loading and unloading, tides, waves and storms had to be considered. Further criteria were highest availability as well as smooth transmission – and without electromagnetic pollution.
Last, in an emergency – for example, a tsunami - the connection needed to be able to be disconnected in a planned manner so that the power is immediately and automatically switched off.

Solution

igus recommended the use of a heavy-duty energy chain, which turned out to be the perfect solution for the application.
The offshore energy chain is attached to the mooring post on the jetty side with a pivoting bracket and to the side of the FSU with a removable extender crossbar.
The robust and flexible energy chain system guides and protects two medium-voltage cables. The heavy-duty plastic chain impresses with its firmly screwed cable guide and interior separation, and is made of special plastics for extreme applications. All tensile forces are absorbed by the inner-lying ropes.  The use of this special energy chain allowed a passive design without the need for mechanical elements due to the continuous movement of the FSU.
The decisive factor was the controlled bend radius of the energy chain, which protects the cables from excessive bending even during a storm. The cables are equipped with special 3-phase medium voltage connectors. The most important safety element, however, is the emergency shutdown. Martin Tiling, Industry Manager Shore Power at igus, explains how it works: "In the event of an emergency, we measure the chain length. If the FSU drifts before it is disconnected from the system, the system will first send out an alarm and then initiate the emergency shutdown. After the power supply is switched off, the shore-side connection point of the energy chain can be pulled out of the special attachment point without the risk of an emerging arc.
"We contributed our expertise in safety and electricity, while igus was able to contribute its experience from challenging cable management projects. "
 
Christophe Gaigneux, Shore Connection Consultant at Schneider Electric

A major multinational project

Looking back on the first energy supply project of this kind at an FSU, Laurent Crémillieux reflects: "It was a real challenge, but we worked on it and found a solution that fits perfectly. We have met customer expectations by developing something truly new and delivering a fully functional turnkey solution."
Apart from the challenges of developing a technical solution, the distance between the partner companies during the project was also a hurdle that had to be overcome.  Schneider Electric's shore power centre of excellence is located in Grenoble/France, igus is located in Cologne/Germany and Schneider's project management and planning teams were based in Korea.
The installation of the state-of-the-art technology took place in Bahrain in June 2019. Three months after the construction was completed, the FSU vessel arrived and was connected to shore power. Currently, Schneider Electric engineers support operations at the site and monitor the electrical system of the complete jetty. This project has demonstrated the benefits of shore-side electricity technologies in the LNG industry. Schneider and igus continue to work on new solutions to standardise the implementation of shore power connections in new industries.
Step 1
Step 2
Step 3
Step 4
Step 5
Step 6


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG