Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Trouble-free despite dirt

Energy chains and bearing technology from igus are used in roller table of Haas Maschinenbau GmbH

Profile

  • What was needed: Energy chains and bearing technology from igus
  • Requirements: Heavy dirt in the form of aluminium and wood chips as well as fine dust from composite materials, torsion  and twisting forces in the system
  • Industry: Machine tool manufacturing
  • Success for the customer: The application is trouble-free in use, no maintenance effort and low costs for the customer
Haas Maschinenbau GmbH
Haas Maschinenbau GmbH is a family business that manufactures both individual components and entire machines individually according to customer requirements. For a current customer project, the machine manufacturer designed a 10-metre-long roller table that can be adjusted asynchronously in width and in which four hydraulic lifting and lowering vacuum platforms were installed. Both roller conveyor halves are driven separately and enable the transfer and removal of caravan roofs that have been milled to size on an upstream CNC machining centre. After the component has been transferred, additional bends and curves are made along the entire length of the component.
For the energy supply system, however, there was the problem that heavy dirt is generated in the overall system, which affects the individual components. The milling machine produces aluminium chips, wood chips and fine dust from composite materials, which are inevitably introduced into the conveyor system. Due to the long installation length of the roller conveyor, twisting and turning during the change in width was unavoidable; a high-precision guide system using recirculating ball bearing guides would have led to malfunctions and blockage.
All the feared problems were counteracted by the use of energy chains and bearings from igus. The application is in trouble-free operation, which makes the end customer in particular very happy today. There is no maintenance effort for the customer in the complete motion technology. Moreover, it is guaranteed with a simultaneous significant overall cost reduction. The budget was thus met and a follow-up plant with igus products is already on the cards.
Guidage linéaire
Haas Maschinenbau GmbH


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG