Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

One year long test convinces the customer about xiros®


Technical data

  • What was needed: Corrosion-free and lubrication-free ball bearings
  • Requirements: Wear-resistant and corrosion-free
  • Material: xirodu B180
  • Industry: Electronics industry
  • Success for the customer: The long-lasting xiros deep groove ball bearings made of the high-performance plastic xirodur B180 provide an ideal bearing of the rollers for this deburring system for printed circuit boards. They defy the humid environment and are in continuous use after a one-year test run.
Go to CONTAG AG: In order to carry electronic components, a printed circuit board (PCB) is required. The CONTAG AG is a manufacturer of high quality printed circuit boards for the electronics industry. Deburring is necessary to remove the razor-sharp edges created during production. This eliminates the risk of injury during further use of the circuit boards.  
Roller bearing in a deburring machine for printed circuit boards

Problem

The CONTAG AG was looking for a suitable ball bearing for the bearing of rollers in their deburring machine for printed circuit boards, which would withstand thedamp environment for a long time and which would also be wear resistant. In addition, the ball bearing was only allowed to have a minimal bearing clearance at the end of the test. For this, the company tested xiros plastic ball bearings from igus and their metallic counterpart in a one-year comparison test.

Solution

After one year, xiros ball bearings achieved a good result in terms of service life compared to metal ball bearings. The metallic bearing variant, which had to be completely degreased, corroded quite quickly due to the humid environment, became stuck and finally failed. With the xiros ball bearings, hardly any differences in wear and clearance situation could be detected after the end of the test. The plant was completely converted to polymer ball bearings.


xiros guide roller in black for visible parts with fixed flange ball bearings

In search of a complete solution?

Are you looking for the right  guide roller system, that creates the  rolling contact between your conveyor frame and the material to be conveyed as a roller conveyor or can act as a film guide roller? And looking stylish as well? Then igus has the solution:
Rouleau de renvoi xiros noir pour les pièces visibles


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG