Plain bearings in underwater torque tool

The bearing which supports the rotor of this tool is subjected to both rotary and side loads. The tool turns at between 6 and 10 rpm, depending on the load. The drive end of the rotor is supported directly by the shaft of the hydraulic motor, which powers the tool. The rotor is stainless steel and operates in sea water. The tool nose has to fit in an ISO standard "bucket" interface which houses the drive shaft turned by the tool, as well as reaction cut-outs to react the tool torque.

In order to make the tool easy to locate on the drive, the drive socket is sprung. This allows the socket to be pushed into the rotor by the drive shaft. When the tool rotates, the spring pushes the socket onto the shaft when they align. This mechanism uses a considerable portion of the diameter of the rotor.

If a conventional ball or roller bearing was used, the diameter of the tool would be too large to fit into the interface bucket. Also, lubrication and sealing would be both complex and heavy. The solution was to use a pressed-in plastic iglide® bearing.
Explore the iglide® overview page

"Had I used a bronze or similar bearing, it would be both expensive and heavy and would also need lubrication. We own two of these tools, both now over 5 years old and the bearings have had no attention other than routine visual inspection." - Ian Harvey, Tooling Manager at Rovtech


Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 965-2496 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH