Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

drylin® R - Design tips

DryLin® Expert System

Use the Expert System to quickly find out which drylin® linear bearing will work in your application.

Calculate lifetime, clearance, and generate CAD files and RFQs using one simple program.

DryLin® Expert System

Eccentric forces

The 2:1 Rule

When using linear bearings, it is important to ensure that the acting forces follow the 2: 1 Rule (see drawing, right). If either the load or the drive force (F) is greater than twice the bearing length (1x), then a binding or interrupted motion may occur.

If the location of the drive force or load can not be changed, simply increase the distance between the bearings, or create a counterbalance to move the center-of-gravity back within the 2 to 1 ratio.
The 2:1 rule,
1. Floating bearing, 2. Fixed bearing

Mounting instructions

drylin® linear bushings in 03 Design Series offer great advantages in applications with parallel shafts. They compensate for alignment and parallelism errors by their geometry and should be used on the shaft located furthest from the drive mechanism.

The design provides a spherical area on the outer diameter of the aluminum adapter for self-alignment. Reductions in load capacity are prevented, since the shaft always lies on the total projected surface.

Thanks to the even load distribution over the entire bearing, edge loads are not possible with self-aligning drylin® R linear bearings. Even in unfavorable conditions, the load is supported by the entire projected surface.

In order to compensate for parallelism errors between two shafts, the outer diameter is designed to be smaller than the housing bore diameter by 0.2 to 0.3 mm (depending on the size). With the use of mounted O-rings, these bearings have an elastic bearing seat. The overdimension allows for maximum compensation shaft misalignments.

drylin® R self-aligning bearings are delivered hard anodized. These surfaces guarantee the highest wear resistance if the aluminum bearing moves in the housing during compensatory adjustments.
The spherical drylin® adapters can compensate for alignment errors. A hard-anodization protects the aluminum adapter from wear.

With built-in clearances and the use of O-rings, the self-aligning drylin® R bearings from the 03 Design Series can compensate for parallelism errors.
Self-aligning DryLin® R bearings from the 06 LL design series Self-aligning drylin® R bearings from the 06 LL design series can compensate for parallelism errors up to +/- 12 inches (3 mm).


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG