Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
180 Bass Pro Mills Drive
Concord
Ontario L4K 0G9
Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact de PresseVoulez-vous être ajouté à notre liste de distribution des médias ?igus® dans le miroir de la presse |
RoHS Compliance going into the future2014-07-24
Since 2006, the RoHS (Restriction of the use of Hazardous Substances), has steadily tightened guidelines set to limit the values of industrially-necessary, yet potentially harmful substances, including lead, hexavalent chromium, mercury, polybrominated biphenyls, polybromibated diphenyl ethers and cadmium in the manufacture of electronics and electrical equipment. With new RoHS II Standards going into effect July 22, a maximum value of 0.1% of the total product weight is allowed for most of these substances, the exception being cadmium, which will be limited to 0.01%. These standards are similar to regulations that are also in effect in countries such as Germany, Japan, and China, so meeting these material standards is becoming of global importance for manufacturers. Though widely used in a vast array of applications, many metal composite ball bearings contain alloys that are not compatible to these new standards. |