Change Language :

iglide® RN289 as a material with the lowest degree of deformation when used in the form of a guide and motion roller for curtains.
 
B-14595 rollers made of iglide® materials are often used for guiding stage curtains. Due to the stationary load during rest phases, these rollers normally become deformed in such a way that their rolling capabilities are restricted. With the aim of countering this effect, this situation was reproduced in the igus® test laboratory and different iglide® materials were tested with regard to their deformation when subjected to a stationary load over a long period of time.

Quality from the igus® experimental laboratory:
Applications involving high cycle counts, speeds and accelerations or demanding environmental conditions require proven systems providing durable and reliable operation, especially when it comes to energy chains, cables as well as polymer slide bearings and linear systems. igus® conducts tests continuously in the in-house laboratory under real life applications. Every year, we conduct more than 2000 tests on e-chains® and cables, and over 5000 tests on slide bearings . The focus of our tests are tensile strengths and shear forces. Coefficients of friction, wear, driving forces and abrasion under extremely different conditions and speeds. Influence coefficients such as dirt, weathering, low temperature, or impacts and shocks are tested