Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

Tough electric vehicle for off-road use

Reliable and maintenance-free bearing points thanks to iglidur plain bearings

Profile

What was needed: 
plain bearings for adverse operating conditions

Requirements: 
extremely reliable and weather-resistant bearing technology, with low maintenance requirements

Industry: electric vehicles

Success for the customer: 
lubrication-free bearing points that guarantee the vehicle's operational capability even under difficult conditions. 
Electric vehicle from LyteHorse

Problem:

The use of conventional plain bearings would have been too prone to failure in the presence of dirt, salt water and extreme temperatures. The developers wanted to create a vehicle that offers the highest possible reliability.

Solution:

The application of iglidur plain bearings is maintenance-free and lubrication-free even in the adverse operating conditions of this electric vehicle. This makes the bearing points of the vehicle very tough.

Power pack with electric drive

LyteHorse Labs has developed a unique electric vehicle that is suitable for numerous applications. For example, at airports, in mining as well as in warehouses and industrial buildings and in the leisure sector. The vehicle is used for transporting people, carrying a payload and towing trailers. It is available with two or four-wheel drive and handles off-road driving with ease.

Designed for maximum reliability

A way had to be found to reduce the moving parts of the electric vehicle to a minimum and thus increase reliability. We could not achieve this with conventional plain bearings because they are susceptible to dirt, salt water and extreme temperatures. As the vehicle is often used in extreme conditions - desert heat, water, mud, dust - we were even more convinced that reducing the number of moving parts on our vehicle would be a unique selling point. In addition, the vehicle is exposed to strong forces when used off-road. The components must therefore also withstand jumps and impacts.  
Electric vehicle from LyteHorse

iglidur plain bearings performed best in the test

Initially, the vehicle was equipped with metal plain bearings. However, these could not withstand the stresses. As the developers wanted to develop a highly reliable vehicle, the metal plain bearings were therefore not a satisfactory solution. Nylon bushings were then inserted into the vehicle and tested. However, the wear was too high, so the developers did not feel safe using these bearings. So they decided to test iglidur plain bearings. A success. The maintenance-free and self-lubricating plain bearings withstood the harsh operating conditions without any problems.

Here you can find the products used




The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH