Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

Intelligent retraction system avoids failures of industrial robots

Equipping machine tools: close-fitting cables with triflex® retraction module

If industrial robots are to work autonomously, all the components have to be right: in this application example, the automation specialist Atemix was looking for a new solution for the cable guidance to the robot head. The industrial robot for equipping a machine tool was previously equipped with a long corrugated hose that often hung in the work area. To avoid breakdowns, the company now uses a triflex® RS universal module. The system pulls or releases the cable guidance depending on the movement, so that all cables are routed as tightly as possible and as loosely as necessary on the robot.

Profile

  • What was needed: triflex R energy chain; triflex RS universal module
  • Requirements: a solution should be found to avoid the winding or snagging of the long corrugated hose of an industrial robot.
  • Industry: robotics; machine tools
  • Success for the customer: a triflex® RS retraction module releases just as much cable length as required. As a result, the cable guidance is always tight without restricting the movement of the robot.
Retraction module on industrial robots This FANUC industrial robot equips machine tools. It was equipped with a new triflex® RS retraction module.

Problem

The Estonian company Atemix Tööstusautomaatika OÜ deals with the automation of factories, with Industry 4.0 solutions and robot applications clearly in the foreground. For a new project, the automated assembly of a machining centre should be solved using a FANUC industrial robot. And although the interaction of machine tools and robotics is not unusual, this application presented a special hurdle. The cable guidance for feeding the robot head with energy and data was solved using a long corrugated hose. Since it could not be guided close to the robot, the hose regularly hung in the work area during the backward movements and blocked the work process - automation was out of the question.

Solution

In order to prevent the corrugated hose from wrapping itself around the robot or getting caught in the machine when it is being driven in and out, those responsible for the project looked for a new way for the guidance of the cable. The key to success here was the use of a retraction system that pulls in the cables when the robot head is retracted and releases them again when the robot head is in the extended position. The triflex® RS retraction system that is now mounted on the industrial robot enables tight-fitting cables without restricting the movement of the system. The strain on the cables during fast and complex 3D movements is eliminated. In addition, there are no longer any sensitive cable elements in the work area and the previously high risk of failure and complex maintenance work are now a thing of the past.

triflex RS robot Before: The long corrugated hose formed a loop that often hung in the work area. There was a high risk of the cable guidance winding around the robot or getting caught in the machine tool.
Robot with triflex® RS retraction module After: Thanks to the retraction module, the cable guidance fits snugly without restricting the robot's movement.

Here you can find the products used

triflex 3D energy chain

  • Specially developed for multi-axis robots
  • High tensile strength and high flexibility

triflex® RS retraction module

  • One module, space-saving and quick to assemble
  • Integrated fibre rods prevent loop formation


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH