Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
180 Bass Pro Mills Drive
Concord
Ontario L4K 0G9
Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact de PresseVoulez-vous être ajouté à notre liste de distribution des médias ?igus® dans le miroir de la presse |
Easy mounting of ball pins by hand, thanks to the clip-on spherical bearing bushing from igus2015-07-13
The new lubrication- and maintenance-free igubal® clip-on spherical bearing bushing (ZCLM 06-10) from igus can be easily mounted manually. The '06' stands for a ball pin of size M6 and the '10' stands for the plate thickness of the holding fixture in millimetres. A cylindrical bore with 12 millimetre diameter, is all that you will need. "The ball pin is inserted into the bushing, then simply pushed until it clicks into the holding fixture," says Thomas Preissner, Product Manager of the igubal spherical bearings division at igus, while explaining the novelty. "Typical application areas for this are coupling rods, double spherical bearings or other solutions for driving connecting rods. The nice thing is that the designers have great freedom in designing their geometries." Inside the bushing there is a spherical holding fixture for the ball pin, that securely holds it in position. igus offers the matching ball pin in galvanised or stainless steel. |