Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
180 Bass Pro Mills Drive
Concord
Ontario L4K 0G9
Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact de PresseVoulez-vous être ajouté à notre liste de distribution des médias ?igus® dans le miroir de la presse |
Dirt-resistant igus linear system displays wins in long jump2019-06-22
Results in athletics can be confusing for the viewer. Whilst in football it is clear when the ball is in the goal, it is not immediately apparent in the long jump whether the jumper has set a new record. Virtual lines help the audience on TV, but are not visible in the stadium. Armin Margreiter therefore devised a new solution for his certified mobile athletics system. The former national coach of the Austrian long jumpers, together with the laser projection expert MediaLas, developed a system that projects the furthest jump distance in the sand. It consists of three laser diodes, which are aimed at the pit and produce a visible line even in direct sunlight. To move the laser diodes, the developers needed a drive unit that can move to positions over a range of 3 to 12 metres. The system should also be easy to transport. Therefore, the decision was made to use a sliding, lubrication-free and maintenance-free drylin linear system from igus on which the laser moves. It consists of lightweight high-performance plastic and aluminium components that are very easy to transport and set up. |