Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact de PresseVoulez-vous être ajouté à notre liste de distribution des médias ?igus® dans le miroir de la presse

Articles de presse par domaine

Special parts for customers made even faster: igus triples its 3D printing service2019-02-05

New laser sintering printers expand the 3D printing capacity for the production of durable wear-resistant parts

The demand for customised special solutions is steadily increasing, especially for the motion plastics specialist igus. Increasingly more customers are turning to the fast 3D printing service for long-lasting wear-resistant parts made of high-performance plastics. Whether for short-term spare parts procurement, for prototype construction or for the production of lubrication-free small batches. To meet this demand, the Cologne plastics specialist has now tripled its 3D laser sintering printing capacity.

If the user wants to produce an abrasion-resistant special part or a small batch then igus has the right solution with the 3D printing service. Call up www.igus.in/3D-printservice, upload CAD data, select material and activate order. In this way the user – from hobbyists to major industrial customers – can quickly obtain igus's wear-resistant special solution. Most of the components are manufactured using the laser sintering process. In this process, the abrasion-resistant laser sintering material iglidur I3, specially developed by motion plastics specialist igus, is applied on the entire working platform and sintered with a laser. After each work step, the plate is lowered and a new layer applied. "Due to the very high demand for wear-resistant special solutions through the 3D printing service, we have now tripled our capacities with new laser sintering printers," explains Tom Krause, Head of Additive Manufacturing at igus.

Quickly printed complex components
The advantages of the laser sintering process are obvious. The laser sintering printers can produce simple and complex types as well as mobile solutions. "In an installation space of 220x170x300 millimetres, for example, 5,000 plain bearings with an inner diameter of 10 millimetres can be produced per laser sintering system within 30 hours. Laser sintering ensures that we can offer the components not only fast, but also with a higher strength and more cost-effectively than the FDM process," notes Tom Krause. High costs, such as the production of injection moulding tools, are eliminated and possible design changes can easily be made on the computer, whereas in conventional injection moulding, entire moulds need to be changed. In addition, there is no price difference between complex and simple shapes. If the customer wishes to have wear-resistant gears made, he can use the abrasion-resistant laser sintering material iglidur I6, which was specially developed for gears, in the 3D printing service. If a series with up to 4,000 parts have to be printed, injection moulding tools can also be produced in additive manufacturing, which are later used in the injection moulding machine. The advantage here is that the user can freely select the suitable material from more than 50 iglidur materials.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH