Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact de PresseVoulez-vous être ajouté à notre liste de distribution des médias ?igus® dans le miroir de la presse

Articles de presse par domaine

Looking for spectacular solutions in plastic plain bearing applications2018-11-07

The manus award goes into the ninth anniversary – Apply now!

What do an exoskeleton, an electric manipulator arm and a research project on space junk have in common? Plastic plain bearings are used in all three applications and all were chosen as winning applications at the last manus award, which motion plastics specialist igus promotes every two years. Now the starting signal has been given for the application phase for the next edition. The winners will receive prize money of up to 5,000 euros.

The jury's biggest challenge at the last edition of the manus award two years ago was selecting three winners out of 541 entries from 35 countries. In addition to the three winners – an exoskeleton to facilitate assembly work, a manipulator arm that can be used underwater up to a depth of 500 metres and an ejection mechanism for a research object in space – there were many other exciting applications with plastic plain bearings. From 3D printers and sports equipment up to art sculptures. "This selection of different applications alone illustrates the versatile application potentials of plastic plain bearings," explains Tobias Vogel, Vice President and head of iglidur plain bearings & drylin linear technology, igus GmbH. He succeeds Gerhard Baus as a new member of the jury. Mr. Baus was involved in the last eight editions of the competition as the co-founder since its inception in 2003. Now the application phase for the 2019 manus has begun.

The manus award comes with prizes of up to 5,000 euros. Users must submit their entries no later than February 22, 2019 and present the design with a brief write-up as well as photos and videos to the jury. It does not matter whether it is series applications for the industry or just a single piece – the only condition is that there must be at least one built prototype of the presented application available. The winners will be selected by an expert jury composed of members from the fields of science, research and specialist media and will be awarded at the 2019 Hannover Messe.

More information at www.manus-award.com. In addition to the conditions of participation, there is also an overview of the previous winners as well as more than a thousand applications of participants in recent years, which illustrate the variety of interesting and inventive applications.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH