Change Language :

iglidur TX2 with felt seal
The new iglidur TX2 with integrated felt seal was developed for applications in very harsh environments, where high loads, dirt and dust also occur.
Due to the special shape of the bearings, the inserted seal is fixed in the component in such a way that it cannot be lost and protects the bearing position from dirt ingress.

For this purpose we developed the iglidur TX2 seals
iglidur plain bearings are generally insensitive to dust and dirt. The greatest challenge, however, lies in corrosion protection. The ingress of dirt can damage the anti-corrosion coating of the used shafts. The consequence: rusted shafts, which can subsequently lead to extreme bearing wear.
igus has developed the new integrated felt seals for iglidur TX2 plain bearings especially for use in high-load applications. They reliably protect the heavy-duty bearings from dirt and dust and ensure lubrication and corrosion-free operation.