180 Bass Pro Mills Drive
Concord
Ontario L4K 0G9
Especially in medical technology and in the laboratory area, the issue of freedom from lubricants and maintenance plays an important role. Other igus® products, such as pre-loaded linear systems, backlash-free lead screw nuts, FDA-approved materials and particle or abrasion-free materials for cleanrooms, can show their capability in this complex environment. Added to this are the requirements for freedom from corrosion, which can also be fulfilled with these systems. All products described are standard parts from the catalogue. They are usually available at short notice. Special parts are also possible if required.
It took around three quarters of a year from development to commissioning of the IVD filling system that works under cleanroom conditions. "We knew right from the start that we would rely on the lubrication-free drylin® linear products due to the requirements on site. They have already proven themselves many times over," concludes Christian Baumann. Manfred Rüdinger adds: "Dust is our greatest enemy. Under no circumstances may dirt be allowed during handling that could falsify tests. And in this case this is 100 percent guaranteed. “
"We have been developing and designing medical devices and system solutions for many years. The focus is on analytical medical technology," explains Dipl.-Ing. (FH) Christian Baumann of the engineering office bearing the same name in Herbolzheim. "Thereby our spectrum ranges from single devices to serial devices of small, medium and large quantities. Precision and reliability are their hallmark. As a matter of principle, we only use fully developed and proven components in order to always achieve the best possible results that prove themselves in the medical environment over the long term. " 2 "We have been developing and designing medical devices and system solutions for many years. The focus is on analytical medical technology," explains Dipl.-Ing. (FH) Christian Baumann of the engineering office bearing the same name in Herbolzheim. "Thereby our spectrum ranges from single devices to serial devices of small, medium and large quantities. Precision and reliability are their hallmark. As a matter of principle, we only use fully developed and proven components in order to always achieve the best possible results that prove themselves in the medical environment over the long term. “
The engineering office has been relying on polymer bearings and linear guides from igus® GmbH, Cologne for many years. There are several reasons for this: First, the focus is on freedom from lubricants and second, the reliability of the machine elements. In this context, their ease of maintenance in operation also plays an important role. If, despite everything, problems should occur, it must be possible to replace the relevant components quickly and easily. Nobody can afford long plant or machine downtimes and the resulting costs. "But in this regard, we have had only the best experience. Over the years, we have never experienced any failures in any area," says Christian Baumann.
The engineering office knows the plastic products from the ground up. "Over the years, we have been provided with many sample parts," says Christian Baumann.
"This is more than helpful with our complex designs, because in the run-up to a new development, by simply trying out the elements that are available we can already have a feeling of whether a component is suitable for the respective motion profiles and will probably stand up to the requirements. And if there is ever a problem or question, a phone call is enough to get quick assistance. “