Injection molding machines

Assembly of plastic injection molding machine
  1. energy chain, various cables like data cables and media cables in injection unit
  2. energy chain, different cables in "picker" unit
  3. Linear guides in sliding door of the clamping unit
  4. energy chain, various cables like data cables and media cables in the clamping unit
  5. Machine bed
  • The machine bed is the base or the foundation of the machine. The switch cabinets are located here and a drive can also be integrated here depending on the machine. The other units that often can also move are located on the machine bed.
  • The initial part of the original forming process takes place in the injection unit. The plastic is heated and liquefied. This takes place in the so-called screw.
  • The clamping unit is the tool that determines the shape of the plastic product. It is called clamping unit, because the supply of the material from the injection unit can be closed and opened in the meantime. In the clamping unit are two mounting plates (one fixed and one moving) as well as a front plate. These plates are fixed vertically on one axis.

Products for use in injection molding machines

Energy supply chains

Linear slide bearings