Fiber-Reinforced Plain Bearings For
Heavy-Duty Applications

Fiber-wound bearings in heavy duty applications

Developed for very high loads

Composite bearings are a combination of different materials. For this purpose, e.g. mineral materials (glass, coal) are woven, combined with synthetic resins and other additives and sometimes pressed together under high temperatures and pressure.

With our igutex plain bearings, a robust fiberglass fabric serves as the outer shell, while an inner layer optimized for sliding properties reduces friction on the shaft.

The combination of these materials results in high-strength fiber-reinforced plain bearings that are primarily used in agricultural, construction and mining machinery. Since our igutex fiber-reinforced bearings contain solid lubricants, they do not require any maintenance or additional lubrication.

Browse our High-Strength igutex Fiber-Reinforced Plain Bearings


igutex TX1 sleeve bearing

fiber-reinforced bearing igutex TX1


​​​​​​​Data Sheet
Browse Shop

igutex TX2 sleeve bearing

fiber-reinforced bearing igutex TX2


  • Perfect for hard shafts
  • Up to 3.5x more wear-resistant than TX1
Data Sheet
Browse the Shop

igutex TX3 sleeve bearing

igutex TX3


  • For continuous operation at the highest loads
  • For heavy duty swivel applications
Data Sheet
Browse the Shop

Fiber-Wound Plain Bearings in Heavy-Duty Applications

Reliable despite dirt and grime 

All-terrain vehicle The track vehicle from Kässbohrer Geländefahrzeug AG relies on wound igutex heavy-duty plain bearings in the oscillating and tensioning axles. Even when driving through mud, slush and bog, the igutex plain bearings are reliable. 
Learn more

Lubrication costs saved

Oscillating axles The Demarko company uses igutex fiber-reinforced plain bearings in oscillating axles for semi-trailers. Since the bearings do not have to be lubricated and are part of the igus standard range, Demarko was able to reduce production costs. 
Learn more

20 tons load and salt water

A-frame The A-Frame from Ship & Yacht Engineering Ltd. can lift loads up to 20 tons. Therefore, heavy-duty plain bearings that are suitable for high loads were required. For use on the high seas, they should also be weatherproof.


Application Assistance

For further questions or product information, please contact:

Photo
Kevin Wright

Country Manager, Canada

Email

Customer Service:

Monday to Friday from 8 am - 5 pm

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH