Change Language :

igus® strain relief systems are specifically designed for e-chains® and other dynamic applications. Combining chainflex® cables with chainfix® strain relief components, these systems deliver high cable durability and exceptional retention force.
To meet a wide range of application requirements, igus® offers cost-effective strain relief solutions that balance performance and value. Tested extensively under real-world operating conditions, igus chainfix® strain relief systems have been trusted by customers worldwide for many years, providing reliable cable protection and long service lives.

In automated machinery, cables face constant mechanical stress with every movement. That's why proper strain relief is critical — it helps secure cables within e-chains®, reducing wear and tear while improving safety, reliability, and system performance.
This free white paper explores the key strain relief technologies and explains how selecting the right solution can maximize efficiency and durability in demanding industrial and automation environments.

A series of in-house tests have shown that a small distance between the strain relief and the bend in the e-chain has no negative impact on the durability of chainflex cables. It is therefore possible to integrate a strain relief for cables directly into the mounting bracket. We offer strain relief options, such as the chainfix clamp or the space-saving tiewrap plates for almost all e-chains.
Strain relief prevents tensile forces from acting uncontrollably on cable connections. This is particularly important in dynamic or heavily stressed applications to prevent damage such as cable breakage or vibrations and shocks.
The right strain relief offers several decisive advantages:
A cable feed-through with strain relief fixes the cable in the cable gland or in the plug-in connector. The strain relief ensures that external forces are not transferred to the cable and are instead absorbed by the structure on which the strain relief is assembled.
The forces at the contacts in the connector or in the cable are then zero. No matter how much the cable moves on the outside, it is at rest on the inside. This protects the contacts and sensitive electronics.
To ensure the optimum performance of energy chains, the following criteria should be taken into account:
igus has established itself as a leading supplier of cable carriers and accessories and offers numerous unique selling points that play a decisive role in the choice of cable strain relief. Here are the main reasons why strain reliefs from igus are the better choice for many applications.

Customer Service:
Phone: Monday to Friday from 8 am - 5 pm
LiveChat: 24 hours
Book a Call
Book an Appointment with a Product Expert