Change Language :

Proper cable installation is crucial to achieving maximum cable performance and extending service life. Following a few simple, easy-to-implement installation best practices can mean the difference between thousands—or even millions—of cycles of reliable cable operation.
In this guide, we’ll explore 7 quick and effective rules for installing cables correctly in your next application to help avoid premature wear and costly downtime.
Before beginning the installation process, many cable manufacturers and industry professionals recommend allowing cables to “relax” for at least 24 hours. This cable relaxation period helps release internal stress caused by prolonged storage on a spool or reel.
However, in today’s fast-paced environment, engineers and technicians often face tight project deadlines, limited resources, and multiple responsibilities. While taking the time to relax cables may seem like a luxury, it plays a critical role in ensuring optimal cable function and longevity.
With chainflex® cable, it is not necessary to waste time laying or hanging cables before their installation. Instead, use the following guide to ensure the performance of your cables quickly and easily.
Proper installation of cables inside a cable carrier system is critical for maximizing performance and preventing premature wear or failure. Follow these best practices to ensure safe, efficient, and long-lasting cable operation.
Always unspool cables by allowing the spool to roll naturally. Never pull cables from the flange or uncoil them from the top. Improper unspooling creates unnecessary mechanical stress that can shorten cable life.
Certain jacket materials can stick together, causing abrasion during movement. Always verify:
Cables should be cut to the appropriate length and laid directly into the cable carrier. This ensures:
Each cable should have enough room to move freely during carrier operation. This helps:
Cables must rest within the neutral axis of the cable carrier, especially when the carrier operates at its maximum bend radius. This positioning prevents tensile strain and reduces the chance of failure during repeated motion cycles.
Installing cables or hoses of varying diameters? Use interior separators or shelving to prevent tangling. Follow these rules:
Always use strain relief on both ends of the cable. This can include:
Customer Service:
Phone: Monday to Friday from 8 am - 5 pm
LiveChat: 24 hours
Book a Call
Book an Appointment with a Product Expert