3 Misconceptions about Thin-Walled Bushings
thin-walled plastic bearing vs. thick-walled bronze bushing
1.1 iglide® plastic bushings have a thin wall, while bronze bushings typically have a thicker wall.

There are a number of instances where an application would benefit from using a thin-walled plastic bushing in place of a thick-walled bronze bushing.

thin walled plastic bushing
1.2 A thin-walled plastic bushing weighs significantly less than a thick-walled bronze bushing. Click to enlarge graph.
thin walled plastic bushing
  1. A thin-walled plastic bushing is not as robust as a thick-walled bronze bushing. The wall thickness of either bushing does not directly correlate to its strength. Other factors that are more important and should be taken into consideration include the weight, coefficient of friction and wear capabilities of the bushing.
  2. Due to its thin wall, the surface pressure of a press-fit plastic bushing will be negatively affected. The surface pressure of a press-fit bushing is defined in pounds per square inch (PSI), which is calculated by load using the formula pounds / (inside diameter x length) and is not dependent on wall thickness. Whether a thin-walled plastic bushing or a thick-walled bronze bushing is used, the surface pressure is solely based on the calculated PSI.
  3. A thin-walled plastic bushing has a shorter life than its thick-walled bronze counterpart. It is reasonable to assume that since a plastic bushing has less material (a thinner wall); it will not last as long as a thick-walled bronze bushing. This is incorrect because the thin wall of a plastic bushing helps to dissipate any heat buildup, which actually prevents wear.

  4. Bronze bushings are designed with a thicker wall to compensate for wear, but even with the added material, the bushing surface is still susceptible to wear. In high-rotation applications, continually re-lubricating the bushing will help prevent wear. However, if a bronze bushing is being used to facilitate other types of motion; excessive wear can lead to added clearance between the shaft and the bearing. If this happens, a number of problems will arise.

  5. It is important to remember that wear is dependent on the makeup of the bushing material and not on the wall thickness (also refer to misconception 1). For this reason, igus® is constantly developing new plastic materials, which minimize wear and provide a long-lasting, maintenance-free solution for a variety of applications.

bronze bushings
1.3 Even though bronze bushings have a thicker wall, they still have higher wear rates than thin-walled plastic bushings.

Contact Us

Questions or product information? Please contact:

Customer Service