Change Language :
Have your e-chain® recycled at the end of its life cycle with the igus® Chainge® recycling program.
This was triggered by specific projects in the semiconductor industry. A cleanroom-compatible energy supply was required for travels of over 30 meters with particularly quiet operation and the highest requirements for particle avoidance. This could not be achieved with conventional sliding solutions. We asked ourselves how we could guide an e-chain over long travels without gliding. That was the starting point for the combination of e-spin and our C6 cleanroom e-chain.
Michael Otrebowski: "One of the biggest tasks was to enable extremely smooth and strong movement over very long travels. To do this, we needed precise gearing to guide the support wheel. My previous work in the field of gearbox technology at igus has helped enormously here. This expertise was crucial for designing the tooth contour in such a way that it engaged cleanly and unrolls evenly. I was also able to draw on the extensive igus® product range of tribo-optimized plastics, which means we can now even achieve the highest cleanliness class."
This solution was originally developed specifically for cleanrooms. The principle is also suitable for many other sectors. We see great potential in the seventh axes of robots, linear robot axes and other systems with variable-length axes. Another market for our e-spin solution is applications where long travels and smooth running are required, such as large format printers. In the past, oversized energy chains were sometimes used here in order to be able to transport a relatively small amount of cable over a longer distance.
Michael Otrebowski: "We roll instead of gliding with defined guidance. This keeps the movement smooth and quiet over the entire distance. The support wheels prevent the upper run from sagging and the tooth contour stabilizes the movement. This ensures controlled, smooth running even at very long travels. The combination of the e-spin with our C6 cleanroom chain is so abrasion-resistant that we achieve ISO Class 1 - confirmed and certified by the IPA Institute."
e-spin creates planning security and flexibility: the attachment height remains constant across all lengths. Up to now, an unsupported e-chains have often been used for smaller axis lengths. From an axis length of around 10 to 12 meters, a sliding solution with a guide trough is used. This has led to various configurations of the system. There is also a critical area in which the travel is too long to be unsupported and not yet ideal for gliding, because the e-chain does not yet settle properly in the guide trough. With the e-spin, system manufacturers will no longer have to make any compromises in future. The same configuration can be used all the time, and the e-chain can be designed to be smaller. This reduces the number of versions, simplifies design and speeds up project processing - regardless of whether the travel amounts to 5, 10, or 30m.
For users, the focus is on operation and suitability for everyday use. The e-spin runs particularly quietly, does not require a guide trough on the floor and is easy to install. As the system rolls instead of gliding, wear is significantly reduced. The result is a virtually maintenance-free, durable energy supply with consistent motion sequences and high process reliability over its entire service life.
Smooth, safe operation on long travels of up to approx. 30m - without guide trough
Constant attachment height for all axis lengths reduces number of versions and design costs
Maintenance-free, durable energy supply system with consistent motion sequences and high process reliability over the entire service life
E4Q series energy chains have been developed to offer the best possible solution for unsupported and long travels. Based on the robust E4.1 energy chain standard that has been proven for over 12 years, the new series brings a long service life and a high degree of modularity.
Typical application areas: machine tools, cranes, automation systems


Customer Service:
Phone: Monday to Friday from 8 am - 5 pm
LiveChat: 24 hours
Book a Call
Book an Appointment with a Product Expert