Boat Lift Manufacturer Uses
Plastic Bearings

A leading boat-lift manufacturer based out of Florida uses iglide® plastic bushings on its lifts to remove boats from the water. The maintenance-free lifts are used by both residential and commercial marinas, as well as private owners.

There were a number of challenges to consider while searching for bearings to use, such as saltwater, mineral deposits, gunk—pretty much anything that floats in the water can get into the lift and affect its components.

iglide® P replaced bearing blocks which had required regular greasing. This task was extremely difficult for customers, and often unsafe — as this maintenance routine required boaters to climb on top of the unit. The grease also contaminated the water and was not an environmentally friendly solution.
Boat lift
Self-lubricating iglide® bearings eliminated the need for maintenance and no longer pollute the water with oil. They are also corrosion resistant. Depending on the boat lift, up to 20 iglide® P plastic bushings are used in the cable-winding drive shafts, which enable the up-and-down motion to fully raise a boat out of the water. iglide® P offers low moisture absorption, low wear, and a high load capacity—which is important, since the boat lifts can handle anywhere from 4,500 to 66,000 pounds with ease. iglide® P also withstands radial loads of up to 1,000 pounds apiece when the boat lift is in operation.
Download the PDF version of this application story

Browse Applicable Products

boat lift bearing application, iglide P

iglide® P sleeve bearing

  • No moisture absorption, even with high ambient humidity
  • Low wear rates
  • High load capacity
  • Cost-effective
Shop now

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 965-2496 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH